This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24630: STAT1 is on without battery connected, but does not charge

Part Number: BQ24630

The circuit is designed for a 6 cell LiFePO4 battery, with ISET1 at 6A, ACSET at 7.85A, and ISET2 at 0.6A.

When I plug in the AC power, without the battery connected, the STAT1 LED glows. We have added a total of 20uF capacitors across the battery terminal. When I connect the battery, the STAT1 LED still glows, however, no actual charging takes place.  The voltage measured across the battery terminals doesn't increase.