I have a functioning BQ77915 cell balancing circuit. I just need to implement / increase the over-current discharge current limit for my existing design. With my existing circuit, I can implement the discharge over current upto 29A. I would eventually like to increase that to 50A or more.
My existing design components for BQ7791502: Rsense: 1mOhm ; ROCD:383kOhms for 180 ms programmable OCD delay
Other than changing Rsense, is there any other way to increase the discharge over current limit.?