This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62568A: Typical switching frequency value for each load conditions

Part Number: TLV62568A


Hello team,

I received a question from my customer about the switching frequency of TLV62568A.

<Question>

Could you tell us typical switching frequency value of each load conditions below?

Input voltage:5V
Output voltage, Load current

①3.3V, 600mA
②1.2V, 500mA
③1.8V, 200mA

<Background>

I already told them to eye measure from the Figure.17 for the relationship between switching frequency and load current. (Datasheet p.12)

However the customer is checking performance, and would like to hear the specific quantitative values from TI. Could BU give a specific value for each 3 of them? If only eye measurement from the graph is available, then that is fine too.

Best Regards,

Ryotaro Fukui