This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS929120-Q1: Output current questions

Part Number: TPS929120-Q1

Hi 

I would like to ask some output current questions about TPS929120:

In the Datasheet, the maximum current of each output channel is 75mA, but if REF is 4.22K, EEP_REFRANGE is 512, and EEP_IOUTx is 3F, the calculated output current is 150mA.
(1) Can 929120 work normally in this case? Are there any risks?
(2) If it can work normally, what is the output current?