This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28780: Start-up & Brown-in

Part Number: UCC28780


Hello Team,

I am working on the UCC28780 and I am using the demoboard EVM 021 and the Mathcad File to design an ACF. 

I don't understand how the start-up is performed and how the brown-in protection is set up.

On the demoboard, if Vin = 25V, the UCC can start-up through the SWS pin but why there is no Vout until the Vin reach ~ 85V ?

Is it because the UCC check also the Vin through VS and compare it with a brown-in threshold ?

Moreover, how can we set the brown-in threshold ? 

Thank you for your answer.

Best regards,

Maxime