Other Parts Discussed in Thread: BQ34Z100, BQ34110
Hi, I'm using the BQ34Z100 to develop a SoC estimator for 12 V 90 Ah Lead-acid AGM battery. I have developed my own electronic card which works well and after calibration and all the necesarry steps, I am trying to do the learning cycle to update the impedance table and the Qmax of the battery. But I have many problems.
Firstly, 2 months ago, I tried to identify the chemistry of my battery within your database and after doing the cycle you indicated, I got the ID 806 with 18% of error deviation for result. After a long talk with TI support, I just got the information that it was unfortunate but that I should continue with that and see if it works.
Now, I am trying to do the learning cycle, but the problem I have is that it is needed to pass 90% of DoD in the battery for a valid OCV measument to be taken. But for a 90 Ah lead-acid battery, it is very complicated or even impossible to pass 90% of the DoD. So, the impedance table update fails because the gauge does not see 90% of DoD passed.
So I was wondering:
- if the impedace table does not update because my equivalent chemistry is too far from the true battery I have ?
- if the impedane table does not update because 90% of DoD is not passed, and if so how to do without that constraint ?
- is the BQ34Z100 appropriate for a large AGM battery ?
So far, when I am using the gauge, the coulomb counter works well but every time a OCV measument is taken, the SoC is readjusted at a value which does not make sense, certainly because the impedance table or the chemistry of the battery is wrong.
Thanks in advance for your help, the BQ34Z100 is a critical component for my PhD and my company so I hope you can solve that issue.
Lucas