Other Parts Discussed in Thread: LM5145
I start a simulation with the Webench for the LM5117. When I try to export the design in ORCAD format I have failed 5 times and more. What can fix it?
I need to design DC to DC with the following parameters:
Vin ~ up 65V.
Vout 5V @ 5A.
Efficiency ~> 80%
The part number should be in stock or in availability in 4 weeks maximum!