Hi, I have a system of 14 cells and the group of 5 cells (vc5 to vc10) is draining more current than the other two groups.
In the beginning, I had bad measurements on this group of cells, I replaced the CAP2 to VC5X and the measurements are ok, but now the draining on this group is excessive.
I connected an array of 14 2.2k resistors in series to simulate the cells and the voltages that the BQ76940 is reading in mV are the following
Cell 1 | 3905 |
Cell 2 | 3819 |
Cell 3 | 3819 |
Cell 4 | 3849 |
Cell 5 | 3853 |
Cell 6 | 2627 |
Cell 7 | 2793 |
Cell 8 | 2775 |
Cell 9 | 2787 |
Cell 10 | 2751 |
Cell 11 | 3810 |
Cell 12 | 3825 |
Cell 13 | 3800 |
Cell 14 | 3857 |
As can be seen, the voltage from Cell 6 to Cell 10 is considerably lower as if there were a resistor in parallel of around 6k for each of these cells or a 30k resistor connected between VC10 and VC5
This means that the BQ76940 is damaged or it could be any of the external components like the thermistors filter capacitor or the RC filter for VC10x or VC5x?