Other Parts Discussed in Thread: UCD9090A
Hi,
I am new to this type of health monitor and would like to know/verify some hardware things. ( without operating evaluation board.)
- For the UCD9090QRGZRQ1 I did not understand how many GPIO function as output only, it can support.
23 is total. 2 can be input only. 10 can be used as rail sequence. What about the rest 11? Can’t they be GPO digital outputs with logic behind them ? please refer to my attached schematics to see the intended use. In the schematics 12 use to control ON/OFF of dc-dc/LDO other 2 use also as outputs (digital) 3 optional.
- Regarding the number of monitors: the UCD9090QRGZRQ1 have 11 monitors but the datasheet states 10 pg2. can’t I monitor voltages of 11 inputs? If it is only 10 on what pins the 10 located from MO1 to MON11? (I mean for voltage monitoring only, without the more sophisticated functions like margining.)
- The Dc-Dc or LDO I use have power good signal (PG). Can I use the GPI as an input to check the status of the PG and combine the GPO controls of power sequencer, when both the 11 monitors and the PG participate in the logic ?
- Can I use the reset pin to power cycle the card, using the FPGA ? in normal operation the RESET pin will be held pulled up by the resistor. When the FPGA (open drain output) will go low (as long as the FPGA is powered) the UCD will enter reset state and thus will shut down the power and rise it up again. Do you see that feasible?
- I intend to use one of the GPO as reset out to processor and peripherals. (SEQ_POR_RESET in schematics)
- This pin should be low during power up and be delayed for minimum 2mS after all voltages stable. Can I make this reset +delay a combination of monitors & GPIs?
- At power down, the Ti processor request that the reset will be prior to the decay of 3.3V and other voltages. In order to match this, I have to detect the falling of the 12V feeding the 3.3V DC-DC. That is why the 12V is monitored.(MON10) Thus, when the 12V will go down below predefined value, the Reset out pin will go low and stay low till the 3.3V decay.
Is that feasible? Can the logic behind the reset out pin can be programmed for different functions when power up and for power down ?
- Can you please review my schematics and comment if something should be changed or taken care of ?
Thanks
Avnerpower_sequencer.pdf