This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65313-Q1: will it work with 5V power supply

Part Number: TPS65313-Q1
Other Parts Discussed in Thread: TPS65653-Q1, , AWR1843, LP87702-Q1, LP87524-Q1

Hi There,

May I check with you whether device TPS65313-Q1 could work with 5V power supply? We are trying to use TPS65313_Q1+TPS65653-Q1 for AWR1843 power supply solution. 

From the datasheet of TPS65313-Q1, it seems the input voltage range is from 4V to 36V. But chapter 6.3 "Recommended Operation Condition", it shows minimum power up input voltage is 5.8V...

and the supply voltage monitor will consider 5.8 ~ 6.6V is UV. In my design, ENDRV/nIRQ is not used. So I assume even with this UV condition, it has no impact to me. 

  

So I want to confirm with you:

1. will TPS65313-Q1 work if the power supply is 5 V?

2. if there is no external MCU to do any SPI config to TPS65313Q1,  could it still provide 3.3V,1.8V normally? I understand the ENDRV/nIRQ is not usable in this condition as the chip will stay in "SAFE" state.

Thanks and Best Regards

Dong