This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ23610: as Inverting buck boost converter for -5.5V at 9A

Part Number: LMZ23610


Hi Dear,

           Can I use LMZ23610 as IBB with input range 9-36V and output will be -5.5V at 9A?

If it is possible can you provide any reference application note?

I have tried using Webench but it says that it is not possible using this.

Thank you 

Kind Regards:

Mohsin