This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25890: technology discussion

Part Number: BQ25890

Dear:

I saw  that BQ25890  could support USB C/PD compatible, what is the compatible ? in BQ25890 datasheet, there is no USB C or PD ,so the mean is BQ25890 can support USB C /PD composition , yes or no ?I need you give me suggestion ,many thanks~

2. what is the DSEL output current ?  can it drive a LED light ?  

  • Hi,

    1. The BQ25890 can work with 5V 3A input USB type-C charging, but chargers can’t detect Type-C. A USB interface is needed.

    2. DSEL is an open-drain D+/D- multiplexer selection output. The max output sink current is 6mA.

    Thanks,

    Ning.