Other Parts Discussed in Thread: LM51561, LM5122, LM5170,
Hi,
The customer configured the schematic with the specification below. However, there is no output.
I don't think it's possible with WEBENCH test.
Is it possible to implement with LM51561 products?
Please recommend a product that is possible.
Spec :
Topology Boost
Vin : Typ 12V(6V ~ 18V)
Vout : 48V
Iout : continuous 10A