This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24650: Simultaneous charging and power supply problem to BQ24650RVAT

Part Number: BQ24650

Hi,

necesitaria vuestra ayuda. yo tengo una placa de bateria con un BQ24650RVAT, apra la carga de bateria ion-litio. El problema esta durante el dia, cuando las baterias estan cargando y el equipo que es alimentado por la placa de bateria  .Muchos de los perifericos del dispositivo dejan de funcionar bien durante las horas de carga solar y por la noche funcionan perfectamente.

I think the problem may be during the charging process of the batteries, because the BQ24650RVAT is not able to supply the necessary current to charge the batteries while simultaneously powering the equipment.
I would appreciate your help.

Thank.

  • I need your help. I have a battery board with a BQ24650RVAT, for lithium-ion battery charging. The problem is during the day, when the batteries are charging and the equipment that is powered by the battery board, many of the peripherals of the device stop working well during the hours of solar charging and at night they work perfectly.

    I think the problem may be during the charging process of the batteries, because the BQ24650RVAT is not able to supply the necessary current to charge the batteries while simultaneously powering the equipment.
    I would appreciate your help.

    Thank.