Part Number: TPS65150
Other Parts Discussed in Thread: TPS65131
Hi,
We are using TPS65150 in our board. Attached the schematics of our design.

The set values are below.
Input : 5V
AVDD: 8.2V
VGH : 22V
VGL :-7
Currently we are facing issue with output voltage.
We are getting 5.4V at AVDD instead of 8.2V and VGH and VGL voltages are coming near to 0V.
As per the datasheet, the Switching frequency is 1.2MHz, but when we probed the SW pin, the frequency is 14.6 MHz.
Please help us to understand the cause of this issue and us to solve this issue.
Regards,
Shafeeq