Hello,
we boughts a few thousands of BQ24041DSQR from your online store - so we can exclude a problem of fake / conterfeit chips.
However, approx. 5% of the chips are not working properly, on a stable project where we didn't have any issue before:
- most of the issues is that the battery charging does not start. PG is asserted, but not CHG, even though a mid-charged battery is connected and VIN is within valid range.
- more rarely, the charging current is invalid. For R_ISET = 4.3kohms 1%, we have a charging current of 83mA, which is largely out of spec.
In all cases, just replacing the chip solves the problem, so there is definitely something going on with the chip.
Do you have a known case of bad chips for this reference?
Thanks,
Florent