Other Parts Discussed in Thread: PTD08D210W, UCD7242, PTD08A020W, UCD7230
This question applies to the following Digital Powertrain modules:
PTD08A010W
PTD08D020W
PTD08D210W
All three of these modules specify a maximum operating temperature of 85C. All three have analog temperature sense outputs.
The PTD08D210W datasheet refers to the temperature being transduced as a "Junction temperature". This analog output reads up to 125C. The other modules do not specify where this temperature is read from.
Can I assume that the maximum specified temperature (85C) is an ambient temperature and not a junction temperature?
If this is the case, then what is the maximum recommended junction temperature (or temperature as read out on the TEMP or TSense pin) for these modules?
Best regards,
Eamon Egan