Other Parts Discussed in Thread: UCC28220, UCC28951
Hi team,
My customer wants to use LM5039 to design a programming DC source.
The design spec is below. Topology =>PFC+ Half-bridge(600W*2 in parallel). Their demands are PWM interleave(maybe use SYNC function) and SR control.
So, My question is LM5309 suitable for this spec or not? if not could you give some suggestions? thanks
Half-bridge (SPEC)
Module1
Vin=400V
Vo=0~80V
Io=0~30A
PO fix =600W