Hi,
Customer has a question about the rise time and fall time of I2C. In datasheet, the max rise time and fall time is 300ns, but didn't show how do we test the rise time and fall time. commonly, 10%~90% is used or VIL to VIH. Could you please confirm this? in customer's use case, if 10~90% is used, then 300ns can't meet.