This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54160 Hysteresis calculation

Other Parts Discussed in Thread: TPS54160

4186.TPS54160.ppt 

Hi All,

We designed DC-DC converter using TPS54160, 24V input(from battery) down to 5V/1A. and one of key requirement is the converter need to turn on at 18V and turn off at 6V. I follow the datasheet(Eq 4 and 5 on page 15) but could not get my target, now converter turn on at 8V and off at 4V. Could you help to review my design in attached? any comment or suggestion?

 

==================================

I used below parameter .

VENA = 3V.

Vstart = 18V

Vstop = 6V

=================================

 

Thanks

NT