This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Load switch selection | 5Vin 5mA Higher ESD

Hi team

Could you help give the correct device to meet this requirement? 

  • VIN=5V
  • Iout=5mA
  • ESD higher than 2kV HBM and 1kV CDM.

Let me know if you have any questions.

  • Hi Shawn, 

    There are several load switches that meet at ESD rating of 2kV HBM and 1kV CDM, but we do not offer any load switches with a higher rating than that. 

    Are you working with a specific end equipment which requires a higher rating? 

    Feel free to email me at e-higgins@ti.com

    Best Regards, 

    Elizabeth