We tie VLDOIN and VDDQSNS together, both inputs = 1.5V, when TPS7H3301-SP disable, there is no glitch on the inputs, but when TPS7H3301-SP enable, output = 0.75V, I find there is a glitch on inputs, it reaches to 1.2V for about 120uS. We have a RC filter between VTT_VO and VTTSNS, we know this makes the output 0.75V overshoot/undershoot nice. But the glitch still there on inputs. It looks like the old TPS7H3301EVM schematic suggests to isolate VLDOIN and VDDQSNS by adding another RC filter R=8K, C = 1uF between VLDOIN and VDDQSNS, but the new TPS7H3301EVM schematic doesn't give a value for the RC filter. I am just wondering if I follow the old TPS7H3301EVM schematic for the RC filter, can we get rid of the glitch on the inputs? if not, is there a way to remove the glitch on the inputs?