Hi Expert,
I want to use UCC39002 to load share with two 20V outputs of DCDC Regulators. I reworked UCC39002 EVB according to figure 5 high voltage application.
The schematics we tested are attached.
The preset circuit goal is that the input voltage of DCDC is 27V and the voltage of shared load terminal is 20.06v. However, in the actual debugging process, the voltage at the output terminal is about 27V, not the 20.06v I set. At present, the voltage measured to VDD is 9.37v, the voltage of triode e is 8.33v, and the voltage of triode C is 27.90v. The voltage at CS + of IC chip is 1.093v, and the voltage at CS - is 2.497v. The test values provided here are from the test 01 circuit diagram. Please help check whether the test 01 circuit diagram is correct.
At present, I have two questions to ask:
Question 1: At present, I use test 01 and test 02 circuits for debugging. The output voltage is close to the input voltage. When the input voltage is 25V, the output voltage is also 25V, which is equivalent to that the current sharing chip does not adjust the voltage and current. Please help check whether the circuit diagrams of test 01 and test 02 are correct? Please correct.
Question 2: How to set CS +, CS -, radj and rsens in the circuit diagram in the high voltage circuit?
Thank you very much!