This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5030: Can VLED be greater than VCC?

Part Number: LP5030


Hi, 

Looking at the ABS MAX table it seems to indicate that the voltage on the OUTx pins are independent of VCC and therefore it would be okay to run the LEDs off 5V (VLED) and the VCC of the LP5030 off 3.3V, but I wanted to confirm this. Is this okay?

Thanks!

John