HI there,
I designed dc to dc buck converting system by LMZ14202H.
In the LMZ14202H datasheet, there are thermal derating verse output current (stating point is 2A) graphs.
The output current in the data begins to decrease by about 80 degrees or more. The temperature didn't drop before that. Does it mean that the efficiency changes according to temperature after 80 degrees? Or does the picture mean a change in maximum capacity according to temperature?
Furthermore, can I get information on the change in efficiency according to temperature with the very small load under as 0.2A?
Regards,
NS You.