Part Number: LM5046
Other Parts Discussed in Thread: LM5045, UCC28950
Hi TI Team,
I have to design a power supply for one of my client with following specifications;-
TI IC used = LM5046
input voltage range = 37v to 57v
output voltage/power = 30v/1000W
switching frequency = 256kHz
efficiency = ~95%
Please resolve my following query;
a. Do you have any reference design fulfilling above specification? If yes then please share.
b. Do you have any excel based design calculation sheet for LM5046 ic? If yes then please share.
c. Do you have any design guide for same? If yes then please share.
d. I have checked and compared the datasheets of LM5045 and LM5046. It seems both are having almost same parameters, pin to pin match and same package. Is it possible to replace lm5045 with lm5046 keeping rest other BOM same?
Eagerly waiting for the reply
best regards
Rizwan Ali