This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM5D1806: tpsm5d1806 sync pin connection in dual and parallel output mode

Part Number: TPSM5D1806


  sync pin needs clock source matching switching frequency requirement from external source or it can be left open?

  • Hello,

    The Sync pin may be left open in a standalone configuration. The sync frequency must be within +/-20% of the internal oscillator's frequency if you are synchronizing the device to an external clock. The internal oscillator frequency is set by the resistors on the MODE2 pin.

    Regards,

    Alec Biesterfeld