Hello team,
I received some questions about overcurrent event of UCC2897A.
For their feasibility study, they are trying to calculate the conditions when overcurrent event occurs, including variation.
Therefore, they want to know the following values and their variations:
(1) What is the CT voltage? (Typical & variation) (Needs for calculating ISLOPE)
(2) What is the CS pin current? (Typical & variation) (Also described as 5 x ISLOPE in DS)
(3-1) What is the Overcurrent detecting threshold of CS pin signal? (Typical & variation) (0.5V?)
(3-2) Minimum CS pin pulse width that would trigger the overcurrent event (Typical & temperature variation)
Detailed information is provided in the attached Excel file. Please check it and contact us if there are misunderstanding about device function or other information needed.
Best Regards,
Ryotaro Fukui