Other Parts Discussed in Thread: PMP9780, PMP
Dear team,
My customer uses PMP9780 reference design for their application, currently we have three questions as below,
1. Our inductor computation is as below. My application condition as below, VIN=3.3, VOUT=6V/-6V, I_load=80mA, and the Ripple factor is 0.2. Then L1=23.6uH, L2=75uH which is too large. Out recommendation is 4.7uH~6.8uH. Our device can't be used under small load current, for example, 80mA? If our device can, then how do I compute the inductor value? Is 10uH enough?
2. Do we have the efficiency of the charge pump design?
3. Below is our BOM, could you please tell me how do you determine the rating voltage of below capacitors?
Thanks & Best Regards,
Sherry