This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMQ61460-Q1: WEBENCH provided converter isn't compatible with Data Sheet

Part Number: LMQ61460-Q1


Hi, 

We are working with LMQ61460-Q1. I can't find this exact part is WEBENCH. The Data Sheet isn't compatible with the converter option that the WEBENCH provides (LMQ61460AASQRJRRQ1).

This is the part that I found on WEBENCH: 

For example, the LMQ61460-Q1 doesn't have a reset PIN according to the data sheet and it has a PGOOD PIN which is missing in the above converter. 

Do you have an option for simulating  LMQ61460-Q1 in WEBENCH? 

Thanks! 

Anna