This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ULN2004AI: ULN2004AI: About RoHS2 compliance

Part Number: ULN2004AI

Are the following products RoHS2 compliant?

Part #: ULN2004AID

Date code: 0436, 0840, 0901

I have confirmed that it is RoHS compliant.

  • Kamijo-san, 

    Yes this device is RoHS2 compliant.

    It seems the distinction between RoHS2 and RoHS is that RoHS2 complaint devices comply with EU Directive 2011/65/EU

    As of right now, all TI devices that are RoHS compliant, also comply with EU Directive 2011/65/EU for Restriction of the Use of Hazardous Substances (“RoHS”)

    Best Regards, 

    Elizabeth