This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25125: Questions for developement support for a mobile bluetooth based sensor device

Part Number: BQ25125
Other Parts Discussed in Thread: BQ25122, EV2400, BQ25120F3A, BQSTUDIO, BQ21061, BQ25155, BQ27Z561-R2

Dear TI power management forum,

I'm planning to use the BQ25125 for a new design of a mobile bluetooth based sensor device. So I have some questions, before I start:

1.) Can I use the bq25210 or bq25122 for testing, or do you recommend a different solution? 

2.) Do I need the EV2400 Interface Board in general for fully testing the chip?

3.) Is there C source code available, which I can use for my controller-firmware?

4.) I'm planning to use a LIR 2477 Lithium 180 mAh 3.6V accu as the power source. Is the BQ25125 the right device for charging the accu?

4.) Do you have any additional informations or hints, which makes the developement easier?

Thanks in advance

With my best regards

Thomas Hülsmann