Part Number: TPS40170
according to TPS40170 datasheet
I don't know the Iripple=1.86A,which one equation i can figure out the value(1.86A)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS40170
according to TPS40170 datasheet
I don't know the Iripple=1.86A,which one equation i can figure out the value(1.86A)?
Hello,
I think you're referring to Equation 20 in the datasheet. Iripple = 1.86A is the inductor peak-to-peak ripple current (which is usually 30-40% of rated Iout at Vin-nom).
See the calculation in Equation 19 for more context where an inductance of 8.5uH is derived. The ripple current is then calculated as 1.86A based on a selected inductance of 8.2uH.
--
Tim
Hi
i know that 30%~40% or 20%~40% of rate current like your description
but rate current 30%(6A) is 1.8A
so follow datasheet ripple current is 1.86A
i don't know that different is from where?
That's the approximate calculation -- the exact result may differ when including MOSFET Rdson and inductor DCR.