This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28881: Light-load

Guru 11170 points
Part Number: UCC28881

Hello E2E,

When light-load opperation onDCM, the switching frequency is not constant. The inductor makes a sound.

Vin : DC350V - DC400V
Vout : 15V
Iout : 50mA(max)

L=3mH

Does it can solve? Or is it normally?

Regards,
ACGUY