This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM51561: Flyback controller selection - LM51561

Part Number: LM51561
Other Parts Discussed in Thread: LM51551, LM5156

Hello,

We are working in PSE design and selecting the components. We have selected LM51561 as boost controller. Our design requirements are,

Vin-18V to 32V DC

Vout -54V,1A (60W) for POE ports

Our questions are,

1) Is the selected controller is best for the application or there is any other suggestion ? How is it different than LM51551 ? Only input voltage rating? 

2) Need help to derive transformer design parameter

3) Can u pls suggest 4 x Port type1 PSE