This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54200: What is the allowable PWM frequency?

Part Number: TPS54200


Hi TI experts,

My customer want to use PWM frequency over 25khz.

When TPS54200 is analog mode, PWM out frequency is 50khz in datasheet. is it right?

in PWM mode, the suggested PWM signal frequency should be less than 1 kHz. this is datasheet comment.

Can TPS54200 operate PWM input over 30khz?

If impossible, could you recommend an LED driver that can input PWM frequency of 25khz or higher.

Thanks,

Downey.