This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63900: The actual impact of cfg resister error

Part Number: TPS63900

Hello Expert,

I have question for this device's cfg feature.
Datasheet recommend to use the resister that has resistance error within 3% including all factor.
Then, I'd like to know about actual concern when I use the resister that violate this required accuracy. Would you tell me it?
For example, there is risk to configure unexpected value or it cannot configure.(e.g, I want to configure output voltage as 2.8V using 10kohm resister but output become 1 step smaller value (2.7V). Or become completely different value).

Best regards,
Kazuki Kuramochi