Hi,
I have some question wants to check as below.
1. Switching frequency only have below can choose? If I want to set 600kHz or 700kHz, any recommend value or figure can reference?
2. In datasheet P22, it recommend set range from 30mA to 200mA, 30mA is the minimum setting per channel?
or I can set this value lower?
3. In "Table 7-6. LED Output String Configuration", this R_LED_SET (kΩ) is not common value, do you have a range table can refence?
or maximum tolerance percentage can reference?
Thanks!
Jeff