Other Parts Discussed in Thread: LM5067
Hi team,
I am debugging our LM5067EVM with following setting
Short JMP1 pin23 and JMP2 pin12 already with Vin input -40V and no load condition.
And the voltage on UVLO pin is -38.02V, so the delta voltage between UVLO and Vee is not over 2.5V.
Have you ever met such a question,if the LM5067 is damaged alreaday or any other possible cause here?
Thanks
Best regards
Mia Ma