Other Parts Discussed in Thread: LM4041-N
Hello,
I use LMV431A in one of our designs and am not sure about maximum case temperature for this device. Maximum power dissipation for this device is in my specific case 40 mW, so far below the maximum allowed dissipation for SOT23-3 case. But I measure 86 degree on the surface of the device.
The derating curve tells me "if there is a temperature higher 85°C, we guarantee for nothing." Am I right here? Or is it possible to ignore this graph and run with a derating of 2.2mW/°C for my case ?
Thanks in advance!
Best regards,
Bastian S.