This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1: Power management forum

Part Number: BQ40Z50-R1

Hello , I'm using the BQ40Z50-R1 do the current sense , the circuit is like below (R19 is two 5 mΩ resistor parallel connect) . the return current have 5~6 mA offset , but is different in charging and discharging, for example ,  2A charging return current value is 2005mA, but 2 A discharging return value is 1995mA , I checked the Rsense resistor was no problem , and also removed the Common-mode capacitance C19 and C20 , the problem still exist , apart from the offset voltage from layout , is there any other reason may cause this problem ? thanks !