My device contains BQ40Z60 with 2s 6Ah battery pack and is in production quite a while. I noticed that after initial battery connection there exists a brief excessive charging current pulse when DC power is first applied to wake the gauge. Charging starts five seconds after DC power application with a one second long excessive pulse, then stops for about 1 second and finally resumes with a normal programmed 3A current. Excess value seems to be device dependent (perhaps due to different calibration constants) and noticed to reach as far as 70% over a normal value. I only was able to make notion of the phenomenon because it rarely briefly triggers overcurrent protection in AC adapter. In all the subsequent DC power applications charging starts normally with no this "probing pre-pulse".
Please let me know if this is an intended behavior or it can be eliminated with fine-tuning?
Regards,
Sergey