Other Parts Discussed in Thread: CSD18563Q5A
Our design has two LM5117 with same caracteristics:
Vin variable between 30Vdc and 42Vdc
Vout 12Vdc
Current Out Max 10A
With no load we have 12V output, but under any load we do not get any output current.
In the past we designed other power units with LM5117 without problems. So this situation is quite upsetting...
Any suggestion or help?