Part Number: BQ25890
1) What does the percentage mean for temperature here?

2) The RTHhot and RTHcold means which value?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BQ25890
1) What does the percentage mean for temperature here?

2) The RTHhot and RTHcold means which value?

Hi,
1) (VTS/VREGN)% may back calculate the thermistor resistance (RTH). RTH can be used to calculate the battery temperature. The battery vendor should be able to provide the equation.
2) In the example, RTHhot = RTH t5, i.e. thermistor resistance at T5=60C (hot). RTHcold = RTH t1, i.e. thermistor resistance at T1=0C (cold).
For RT1 and RT2 calculation tool, please refer to http://www.ti.com/lit/zip/slurax7.
Thanks,
Ning.
There are 2 modes in datasheet. Generally I think it's BUCK mode, but when use boost mode?

Hello,
The charger can operate the buck converter in reverse, turning the buck into a boost with the output on VBUS for OTG applications that require 5V and up to 2.4A.
The charger will use different temperature thresholds in boost mode operation.
Sincerely,
Wyatt Keller