Hi
In TPS2546
1. based on the datasheet table3: truth table, i saw status pin column show off, does it mean status output pin is disable? and can i say status pin will be enable when ILIM_SEL is high?
2.i saw datasheet mention that if ILIM_SEL is always high, we do not care RILIM_LO, does it mean ILIM_LO only work in ILIM_SEL=high condition?
3. from section 6.5, it shows some Ios parameter. In the test condition, it mention ILIM_SEL=VIN and RILIM_HI= 20 kΩ you can get Ios parameter. if my ILIM_SEL=3.3v(not 4.4<vin<5.5), is there different result? i mean RILIM_HI have different value to achieve the same Ios? if it will change, can i know how to fine tune it?
4.for wake up function, i saw datasheet set current limit by ILIM_HI and Ios_pw for no load detect. Can i know where is Ios_pw or how to know it work?