Hi Team,
We can setting LED current level by register 0x00H ~ 0x03H. Does the LED current register setting for IL_max or IL_avg?
Take RLED for example:
We set the RIREF = 16.5k ohm(1.5A) and RLED[9:0] = "0100010001"b(400mA)
the waveform measurement as below.
IL_Max = 410mA (red line)
IL_Avg = 362mA (green lin)
Best regards,
Hardy