Other Parts Discussed in Thread: BQ25619E
Hi. My customer is looking for alternatives to wants to BQ25619E and wants to know the status of BQ24253 and if there are any plans to NRND the device.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Vanessa,
No plans to NRND the BQ24253. Keep in mind that the D+/D- detection locks the input current limit at startup and the input current limit cannot be changed without toggling the EN1 and EN2 lines. On this device. if D+/D- detects a USB BC1.2 SDP, the charger locks the input current limit to 100mA. Is that enough current to power up the system processor until it's GPIOs can toggle EN1 and EN2 to increase the input current limit?
Regards,
Jeff