Part Number: TPS65053
Other Parts Discussed in Thread: OMAP-L138,
Hello, I am using TPS65053 power chip to supply power to OMAP-L138 processor. When the power input of the chip is unstable for a moment, one OF the LDO output will be abnormal. Normally, the output should be 1.8V, but after abnormal, the output voltage can reach 2.7V In an abnormal state, power chip heating obviously,DSP chip heating obviously. When I give the RESET foot of the power chip a low level signal to RESET, the power chip can work normally. The circuit diagram of the chip is as follows:

中文如下(中文):
你好,我在TPS65053电源芯片给OMAP-L138处理器供电,当芯片电源输入突然异常会导致一路LDO,应该正常是1.8V输出,后电压输出可到2.7V,当我通过使能脚来关闭LDO时是无法关闭的,这个控制台系统状态出现异常状态,电源芯片发热,DSP芯片也明确。当我给电源芯片的RESET脚一个低信号信号来复位时,电源芯片正常工作.电路图如下: