Hi,
My customer needs a DCDC to cover these requirements
Vin = 10V to 40V
Vout = 48V
Pout = 480W (!0A)
Efficiency >95%
Do you have any recommendations?
Thanks Josef
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Josef,
There are two options:
The LM5170 will achieve even power sharing between the two phases. The EVM is for bidirectional but you can make if for boost only by grounding the DIR pin and you also need to remove the circuit breaker FETs on the 12V side and bypass the breaker.
Please take a look and we can further discuss.
Thanks,
Youhao Xi, Applications Engineering