Other Parts Discussed in Thread: UCC28780, UCC28782, LM5023, UCC28600, UCC28742, UCC28704, UCC28740
Hi team,
can LM5026 be used in the flyback topology like diagram below? If no, why?

Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello H. Tian,
The LM5026 is an Active Clamp Flyback controller.
The Typical Application Circuit from page 1 of the data sheet is show below.
There are some differences at the output of T1.

The LM5026 data sheet can be found here:
An EVM for the LM5026 can be found here:
Best regards,
Eric
Hello Eric
Thank you for your reply.
I saw the typical application from LM5026 is for forward circuit (so the diffrences at the output of T1). My question is: is LM5026 also suitable for a DC-DC Flyback Converter? You said, "The LM5026 is an Active Clamp Flyback controller". It means, i can use it in my flyback converter circuit? Sorry, i am little confused.
Let me tell you more details about my application: my circuit is a DC to DC auxiliary power supply, i want to improve the efficency by recovering the leakage inductance energy. I want to avoid to use the highside clamp fet, like the typicial application from UCC28780 or UCC28782. Is there any controller for my application?
thank you.
Hello H. Tian,
I have connected with Hong Huang, internally at TI. He is the expert who usually supports this product line. So, I am transferring this thread to him. Thank you, Eric
Hi,
You can use LM5026 in either flyback or forward. My understanding to your need is you want to get a Quasi Resonant controller. If so, you may take a look at LM5023 or UCC28600.
Hi,
You can also consider UCC28740, and UCC28742 for QR flyback. If you can use the primary side regulation you may consider UCC28704.
Hi Hong Huang,
Thanks for the tips. I use the secondary side regulation (the flyback transformer has no auxiliary winding) and my circuit works in CCM mode with a swiching frequency about 200kHz.
Another question: the active clamp flyback use typically highside Fet as clamp. What is the advantage compared to lowside clamp fet?
Thanks
best regards
Hi,
Low-side clamp uses P-channel MOSFET which drive is on the same reference as the LM5026. High-side uses N-channel MOSFET which needs voltage level shift with a gate transformer or a high-side MOSFET driver. Usually P-channel MOSFET cost more than N-channel. But level shift may need to have additional cost. It is difficult to find P-channel MOSFET with voltage rating > 200V, or very expensive.